我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the static load capacity of a NetShelter WX wall mount cabinet?
Issue:
I customer is asking for static load capacity of a NetShelter WX cabinet. It's not noted in the Specification tab on the APC website.

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
A customer needs to make sure they don;t exceed the load rating, or that it meets their needs.

Resolution:

All of the NetShelter WX cabinets have a static load rating of 200 lbs.