我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Does the ATV930 drive have a traverse control function embedded?
Issue:
Is traverse control function a built-in feature on the ATV930?

Product Line:
Altivar 930

Environment:
All

Cause:
N/A

Resolution:
Traverse control is not available in ATV930 drive.  This function is only available in ATV320.