我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to overcome the offset issue in Electrical organisation tab of Ecostruxure Power Design - Rapsody?
The offset issue can be observed in Electrical organisation tab of Ecostruxure Power Build -Rapsody. Whenever try to select the components from the Single line diagram, selected area will be offset from the selection cursor. This issue can be resolved by the below settings in the computer
1. Resolution of the system to be 1366X768


2. Size of text, apps and other items to be set for 100%
3. Orientation should be for landscape