我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Magelis shows error "configuration file is not unicode"
Issue:
The Magelis HMI fails to boot properly and there is an application halt. The error on the dialog states the following:

Config problem:the configuration file is not unicode
KAOScore:PortableProjectConfiguration.cpp:line 406


Product Line:
Magelis HMI programmed Vijeo Designer (any version)

Resolution:
This error is a result of a corrupt Vijeo Designer installation on the PC where the software is installed. To resolve this issue, please re-install Vijeo Designer and re-download to the HMI.