我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
On an ATV320, is there a better way to alleviate motor stalling other than adjusting IR compensation?
Issue:
ATV320 alleviating motor stalling options other than adjusting IR compensation

Product Line:
Altivar 320

Environment:
All

Cause:
Motor stalling

Resolution:
You can adjust the speed loop by setting SPGU parameter when CTT=Standard.
Otherwise, set SPG and SIT parameters when CTT=SVCV.