我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the recommended maximum cable length (with part numbers) for the TM3BCEIP Bus Coupler?
Issue
What cable do I use for the TM3BCEIP Ethernet/IP or Modbus TCP Bus Coupler?
What is the maximum length for the cable(s)?

Product Line
Modicon TM3

Environment
Distributed I/O Modules for M221, M241, M251, M262 PLCs

Resolution
The cabling options for the TM3BCEIP Bus Coupler module are as follows.
All cables listed below are Ethernet Shielded cables for DTE connections with equipped with RJ45 connectors at each end.

For environments without Electromagnetic Interference (EMI), the maximum cable length recommended is 80m. Part numbers are as follows:
CE compliant cables:
490NTW0002 - 2m (6.56 ft)
490NTW0005 - 5m (16.4 ft)
490NTW00012  - 12m (39.37 ft)
490NTW00040 - 40m (131.23 ft)
490NTW00080 - 80m (262.47 ft)

UL compliant cables:
490NTW0002U - 2m (6.56 ft)
490NTW0005U - 5m (16.4 ft)
490NTW00012U  - 12m (39.37 ft)
490NTW00040U - 40m (131.23 ft)
490NTW00080U - 80m (262.47 ft)

For harsh environments with Electromagnetic Interference (EMI), the maximum cable length recommended is 10m. Part Numbers are as follows:
CE compliant cables:
TCSECE3M3M1S4 - 1m (3.28 ft)
TCSECE3M3M2S4 - 2m (6.56 ft)
TCSECE3M3M3S4 - 3m (9.84 ft)
TCSECE3M3M5S4 - 5m (16.4 ft)
TCSECE3M3M10S4 - 10m (32.81 ft)

UL compliant cables:
TCSECU3M3M1S4 - 1m (3.28 ft)
TCSECU3M3M2S4 - 2m (6.56 ft)
TCSECU3M3M3S4 - 3m (9.84 ft)
TCSECU3M3M5S4 - 5m (16.4 ft)
TCSECU3M3M10S4 - 10m (32.81 ft)