我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is it supported to create dynamic message for alarm in VXD/EOTE
  1. Issue
Is it supported to create dynamic message for alarm in Vijeo XD / EcoStruxure Operator Terminal Expert .
  1. Environment
Vijeo XD / EcoStruxure Operator Terminal Expert V3.1.
  1. Resolution
No, It is not like Vijeo Designer, user can’t create dynamic message for alarm in Vijeo XD / EcoStruxure Operator Terminal Expert V3.1.