我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the switching power of Altivar process relay outputs?
This information can be found on product datasheet on web.

Max switching power for AC load is:
2A at 250V AC providing that the load is resistive or slightly inductive with either cos phi 0.4 or better or time constant L/R of 7ms or lower.
Max switching power for DC load is:
2A at 30V DC providing that the load is resistive or slightly inductive with either cos phi 0.4 or better or time constant L/R of 7ms or lower.

施耐德電機Taiwan

附件
Relay.jpg [49.54 KB]