我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to fix the popup window location issue in VJD 6.2 SP9
  1. Issue
In Vijeo Designer 6.2 SP9,the location of popup window in Webgate is not correct, how to fix the issue?
  1. Environment
Vijeo Designer 6.2 SP9.
  1. Resolution
User can upgrade to Vijeo Designer 6.2 SP9 HF4(6.2.9.1702_6.2.9.1701).
The location of popup window in webgate will be correct.
  1. FAQ Applicable Conditions
FAQ applies to Vijeo Designer 6.2 SP9.