我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Where can AR8654 be installed on the NetShelter Networking roof?
Issue:
There are places on the Networking roof where the AR8654 will not install.

Product Line:
NetShelter Networking Cabinets

Environment:
AR3140, AR3340, AR3347 all serial ranges.

Cause:
The Networking roof is different than the standard NetShelter roof.

Resolution:
Please see the attached file for locations where the AR8654 can mount.

施耐德電機Taiwan

附件
AR8654 Installed Onto NetWorking Cabinet.pdf [226.31 KB]