我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to improve the 4G connection on a HMI Box module with a weak signal ?
Question
How to improve the 4G connection on a HMI Box module with a weak signal ?

Description
If you use a Magelis IPC (HMI Modular Box) with a weak 4G signal (like a 2G signal), is it possible to meet some connection interuption due to the weak signal.

After a signal interruption, a device mechanism waits 10 minutes before to try to connect the 4G interface again.

To come back again more faster is it possible to use the script as bellow to activate the APN again :

AT+CFUN=4     //Enter to airplane mode
Wait(5Seconds)
AT+CFUN=1    // Network mode
Wait(30Seconds)
AT+COPS?
AT+UPSD=0,1
AT+UPSD=0,1,\""+apn+"\"
AT+UPSDA=0,3
AT+UPSND=0,0

This script will reduce the waiting time from 10 to 1 minute

Keywords
HMIYMIN4GEU1, HMIYMIN4GUS1, HMI Box Module, 4G, HMIBMI, HMIBMO, HMIBMU, HMIBMP

Case author:
Lilian Cabos

Product Familly
Magelis IPC