我们今天能为您提供什么帮助?

EcoStruxure Process Expert: Guidelines to transition an application from GPL Classic to GPL Situational Awareness

This Knowledgebase explains the steps need to be followed for existing customers who want to leverage the new general process library

Issue

If any existing projects or customers want to leverage the new general process library, they must transition their project to replace the libraries and re-draw their graphics screens as it is a new library, and while functionally like previous general process libraries there is no direct upgrade between the libraries.

Product Line

This document has been created for EcoStruxure Hybrid DCS 2019 and above versions

Resolution

The attached document details the step that needs to be followed for upgrading the GPL Classis to GPL SA.



施耐德電機Taiwan

附件
Guidelines to transition an application from GPL Classic to GPL SA.pdf [648.73 KB]