我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can previous versions of ENM be installed on a PME 2020 system?
Issue
Can other versions ENM be installed on PME 2020 system?

Product Line
Power Monitoring Expert 2020
ENM 8.3.4

Environment
System Notifications

Cause
PME 2020 now installs with a web based ENM. Some users may want the previous versions of ENM's interface and would like to install ENM separately from the one PME 2020 now installs

Resolution
ENM 8.3.4 can be installed separately from the version included in PME 2020. However the installer for ENM 8.3.4 is found in the PME 9.0 .iso file.  A base license will also be required. You can find the PME 9.0 installation files here.

NOTE: While this process can be followed, it is recommended to transition to using the web based ENM that is used in PME 2020 as ENM 8.3.4 is not compatible with subsequent versions of PME