我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Configure the BMXNOR0200 for DNP3 communications with redundant server
Issue
Configure the BMXNOR0200 for DNP3 communications with redundant server

Product Line
BMXNOR0200

Environment
Windows 7, Windows 10

Resolution
The purpose of this video is to demonstrate how to configure the BMXNOR0200 to communicate with multiple DNP 3 servers