我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Unity14-UnityLL984 Library install returns ObjectStore error
Issue
Unity14-UnityLL984 Library install returns ObjectStore error

Product Line
Control Expert 14

Environment
Windows 10

Resolution
Installingt the 'UnityLL984 Library' into Control Expert 14, returns the following ObjectStore error.
efr

To resolve the issue:
  • Unzip and run the attached batch file named 'UpdateRegistry'.
  • Install the 'UnityLL984 Library'.

施耐德電機Taiwan

附件
UpdateRegistry.zip [886 Bytes]