我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Why can’t we see the shadow of objects in EOTE
  1. Issue
In EOTE runtime, why can’t we see the shadow if the object’s width or height is 600 pixels or more.
  1. Environment
EcoStruxure Operator Terminal Expert 3.1 SP1 or later.
  1. Resolution
In version 3.1 Service Pack 1 or later, if the object's horizontal width or vertical height is 600 pixels or more, a shadow will not display regardless of the shadow settings.

(1) Horizontal width
(2) Vertical height

  1. FAQ Applicable Conditions
FAQ applies to EcoStruxure Operator Terminal Expert 3.1 SP1 or later.