我们今天能为您提供什么帮助?

What is accuracy of the external 24VDC delivering by a BMXCPS 200 power supply?

the 24VC delivering by a BMXCPS200 is befine between 23.3Vdc à 24.7Vdc over the entire input voltage range, over the full output load range and over the full temperature range