我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to mount Harmony P6 Box to the Display?
Goals and Symptoms
New Harmony P6 is Modular for enlarged line-up: Each Box is compatible with each Display.
In some cases, customers receive the Box and the Display separately. Also, they will be able to replace the display himself for maintenance reason.
The goal of this resolution is to provide the steps to follow in order to mount the Box to the Display
Causes and Fixes
Here is the video to show How to mount the Box to the Display