我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How many electrical equipment can be connected to Smartlink ELEC?

The quantity of electrical equipment depends on the electrical installation and system architecture.
Smartlink ELEC can connect up to
• 7 digital channels, per channel you can connect to 1 Ti24 auxiliary or 2 pulse energy meters
• 1 analog channel, per channel you can connect to 2 sensors with 4-20mA or 0-10V output.