我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is there a way to get an ATV320 ATV Logic print out in SoMove?

Issue:
Can you print your ATV Logic configuration from SoMove Software?


Product Line:
Altivar 320


Environment:
All Models


Cause:
ATV Logic


Resolution:
There is no print function available for ATV Logic like there is for parameters. Will have to do screen capture is the only way to print ATV Logic