The control port Mac address of the BMENUA0100 module can be accessed by the M580 through modbus (Read_Var) at the following mapping address:

BMENUA0100 Firmware version 1.10.25
BMENUA0100 Firmware version 1.10.25
發佈於: 施耐德電機Taiwan




我們的品牌
歡迎造訪施耐德電機全球網站