我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to download log from the BMENUA0100?
To get the log from the BMENUA0100, you need to log on the webpage module and then follow the step below :
Access to the webpage of the BMENUA0100 :

If the module has his Rotary switch on “standard” security, the login is :
User : installer
Password : Inst@ller1

If the rotary switch has his Rotary switch on “secure, then fill it with the user and password that the customer has defined
Then click on the button “:support info” Download.

support infos file
A pop-up will appear asking a password. The password has to be given to the Technical support and It will be useful to uncryptic the file.

password for support info file

施耐德電機Taiwan

探索更多
產品:
探索更多
產品: