我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is EVlink Pro AC compatible with the TIC protocol and the French smart meter Linky ?

Article available in these languages: Czech

Yes, by adding the accessory board, reference EVA1MTH / Installation guide GEX2219201.
It is connectable to Historical & Standard TIC and compatible with 3-phase or single-phase
The configuration is done using eSetup,(see below) .



eSetup4