How to use the System Backup Scheduler feature EcoStruxure Process Expert ?
This Video explains the System Backup Scheduler feature
A service that helps the user to take the backup of the systems/projects regularly as per the predefined schedule.
The backup can be taken from date, week, and monthly options. With the help of this feature, the EcoStruxure Process Expert would be taking the backup of the system/project automatically as configured by the user.
NOTE: This feature is supported only for EcoStruxure Process Expert 2021 and above versions.
發佈於: 施耐德電機Taiwan