我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
APC Advances to Offer UPS with Lithium-Ion Battery

Traditional lead-acid batteries can cause multiple pain points for customers and their businesses. Take a look at a few of the most common challenges customers face with lead-acid batteries:

  • The weight and size of lead-acid batteries make UPS units difficult to install without two or more people and without the right equipment.
  • Lead-acid batteries have an approximate lifespan of three to five years, meaning you will have to replace them often and risk UPS failures and extended downtime.
  • For businesses with multiple distributed locations with IT systems, maintaining an inventory of short-life acid batteries is costly and time-consuming.

Benefits of APC Smart-UPS Lithium-Ion batteries

APC Smart-UPS products offer many solutions to keep your organization reliably connected.

  • 3x the battery life: APC Smart-UPS lithium-ion batteries can last up to 10 years, with three times the battery life of traditional lead-acid batteries, and can save up to 50% on the total cost of ownership.
  • Easy to install: APC lithium-ion products can be up to 75% smaller and up to 65% lighter than lead-acid batteries, making installation faster and easier than ever.
  • Visibility anywhere: All APC lithium-ion products come with software and network management card connections to monitor energy consumption or shut down safely in the event of an extended power outage.
Finally, every Smart-UPS Lithium-ion unit is backed by a five-year warranty, so the customer has peace of mind knowing that APC is always here to support should there be any issues.

Should you choose to have UPS with a lithium-ion battery, don't hesitate to call the APC sales hotline in your country to inquire.