我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the altitude derating of standard TM5 IO modules?
The altitude derating of standard TM5 IO modules is the same for all TM5 modules but it doesn't mentionned on the documentation.

TM5 environmental condutions:

temperature TM5 IO modules

The TM5 altitude derating is a reduction of ambient temperature by 0.5°C per 100m:

0 to 2000m => No limitations
>2000m => -0.5°C / +100m