我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Uninstalling Eclipse in Ubuntu
RemoteConnect 3.0.3 works with Eclipse version 2022-06 for the SDK on the Edge platform

If a customer is having issues with Eclipse and needs to repair/reinstall it or if they have an incorrect version installed that needs to be removed.

From a terminal window in Ubuntu (Ctl-Alt-T)

cd ~/
rm -rf ./eclipse
rm -rf ./.eclipse
rm -rf ./oecore-i686/

This will remove all of the components associated with Eclipse. Please refer to the SCADAPack x70 Documentation "Installing Eclipse and SCADAPack 47xi SDK" for reinstalling Eclipse and the SDK.