我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
SRTG UPS Reports Self-Test Refused After a Successful Self-Test

Problem: The self-test status of SRTG UPS models reports "Refused" after a successful self-test

ref

Product Line: UPS models with the prefix SRTG

Cause: Due to the current firmware logic, it is expected behavior that SRTG UPS models report "Refused" after a successful self-test. The expected self-test status sequence is Status: In Progress -> Actual self-test screen -> Status: Refused, as shown below:

prog -> prog -> red

Resolution: A future firmware update will improve the UPS self-test reporting.

施耐德電機Taiwan

探索更多
產品:
探索更多
產品: