我们今天能为您提供什么帮助?

How to duplicate the project in EcoSet Design?

You can create a new project based on an existing project.

1. Select the project you want to duplicate.

2. Select Duplicate Project.

delete project

The project is duplicated and displayed.

NOTE: The duplicated project is saved with the existing project name,

appended with the string “copy”.