Is It possible to mix standard powered sensors and two-wire sensors on the 4-5-6 inputs of the STBACI1400 module?
You cannot mix standard powered sensors and two-wire sensors on the 4-5-6 inputs of the STBACI1400 because input 6 serves as the "return" or common for inputs 4 and 5.
For powered sensors, connect input 3 or 6 to the sensor, not to the (-) of the power supply.
EXAMPLE:
For Powered sensors:
For 2 wires sensors:
Best Regards.
發佈於: 施耐德電機Taiwan
Discontinued
To be Discontinued
Discontinued
To be Discontinued