What is the default IP address of the M172 Secure Interface Gateway when connected via USB?
Issue:
Default IP address of the M172 Secure Interface Gateway when connected via USB
Product Line:
M72
Resolution:
The default IP address after the connection of a PC to TM172 Secure Interface Gateway via USB mini-B connector is 192.168.254.254 .