Roll over image to zoom in

SmartX IP Override Display Module, For All MP-C Models
SXWMPCDSP10001
EAN Code: 3606481355492
Direct connection to the SpaceLogic MP-C controllers
Features an LCD display and five keys with resolution of 128 x 64 pixels
Add-on module that provides insight and control of the inputs and outputs
Enables manual override of outputs for testing, commissioning and maintenance
Dedicated processing power for reliable override for maintenance applications
Environmental Data
Environmental Data
Total lifecycle Carbon footprint
6
Use Better
Packaging made with recycled cardboard
Yes
Use Again
Take-back
No