Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are Homeline load centers available for a 3 phase application?
Issue:
Homeline load center for 3-phase voltage system.

Product Line:
Load Centers

Resolution:
No, Homeline is available in single phase construction only. For 3 phase application no more than 240 Vac, consider using a QO Load Center.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings