Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there a transformer that can take a single phase input and create a three phase output?
Issue:
Can a single phase transformer create a three phase output?

Product Line:
Transformers

Environment:
Low voltage Transformers

Resolution:
It is not possible to change a single phase source into a three phase source with a static device, such as a transformer. An active device is required, examples of which are phase converters or some special variable frequency drives.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings