Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does Square D offer generator interlock kits for the combination service entrance devices (CSED)?
Issue:
Product availability

Product Line:
Combination Service Entrance Devices

Resolution:
Yes, BUT the Generator Interlock Kits are available ONLY for certain CSED catalog numbers and the below catalog numbers are the ONLY devices that can be used with a generator kit. Any other CSED catalog number would NOT allow the use of a generator kit.

The RCGK2 can be used with the following catalog numbers: "RC816F_ _ _C" or "RC816F_ _ _CH" and "RC2040M_ _ _C" or "RC2040M_ _ _CH" or "SO2040M_ _ _S". Where the '_ _ _' is the amperage of device.

The QCGK3 can be used with the following catalog numbers: "QC816F_ _ _C" or "QC816F_ _ _CH" and "QC2442M_ _ _C" or "QC2442M_ _ _CH". Where the '_ _ _' is the amperage of device.

The HOMCGK2C can be used with the following catalog numbers: "RC816F_ _ _(S / SH / SL / SS / SLS / SHS)" and "RC2040M_ _ _(S / SH / SS / SHS)" and "RC3040M_ _ _(SL / SLS)" and "RC3042M_ _ _(PS)". Where the "_ _ _" is the amperage and the letters in the ( ) would be potential suffixes of the catalog number.

The QOCGK2C can be used with the following catalog numbers: "QC816F_ _ _(S / SH / SL / SS / SLS)" and "QC2442M_ _ _(S / SH / SS / SHS)" and QC3040M_ _ _SH". Where the '_ _ _' is the amperage of the device and the letters in the ( ) would be potential suffixes of the catalog number.

The QUCUGK can be used with the following catalog numbers: "QU48F_ _ _(PS or PSL)" and "QU816F_ _ _(PS or PSL)" and "QU816M200PS and "CU48F_ _ _PS" and "CU816F_ _ _PS".

The RUSUGK can be used with the following catalog numbers: "RU48F _ _ _(PS or PSL)" and "RU816F_ _ _(PS or PSH or PSL)" and "RU816M200PS" and "SU48F_ _ _PS" and "SU816F_ _ _PS".

NOTE: There are NO generator interlock kits for the 400amp CSED devices.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings