Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Video: Installing PKOGTA2 Equipment Ground Kit on Heavy Duty Safety Switches

Article available in these languages: Spanish

Issue:
How does the PKOGTA2 get installed, what is the torque requirement and mounting screw size for this Equipment Ground Kit?

Product Line:
Heavy Duty Safety Switches

Environment:
Switch accessories

Cause:
Installation

Resolution:
The PKOGTA2 comes with 2 Tang Lugs, 1 mounting screw and 2 labels.
The wire binding screws should be torqued to 200 lb-in.
The mounting screw is a 12-24 x 0.640" hex/slot washer head and should be torqued to 25 - 45 lb/in. The screw is THREAD FORMING screw. Do NOT substitute a SELF TAPPING screw.
To purchase the mounting screw, order part number 4020506501 (1 required).

NOTE: MAKE SURE TO VERIFY THE PKOGTA2 KIT CAN BE USED IN THE SPECIFIC CATALOG NUMBER IT IS BEING INSTALLED IN. Because, the PKOGTA2, Service/Equipment grounding lug is used in several different circuit breaker enclosures and safety switches.
The featured video is ONLY to supplement the INSTRUCTIONS that come with each PKOGTA2 kit.

PLEASE make sure to read and follow the instructions that come with each PK ground bar kit and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.

A PDF of the Instructions for the PKOGTA2, is attached below.
Danger label

Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
Once all Safety steps are followed, begin the kit installation by following the instructions that come with the kit.

Video

Schneider Electric USA

Attachment(s)
PKOGTA2 Instructions.pdf [67.3 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings