Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is the door on a NEMA Type 1(Indoor) Cover for both QO and Homeline load centers, hinged on the right or left side?
Issue:
Will a QO and Homeline loadcenter door open from left or right?

Product Line:
Loadcenter

Environment:
QO, Homeline

Resolution:
When positioned with the mains located at the top, the door itself will be hinged on the Right side (open from the left to right). If the load center in question is rotated 180 degrees, so that the mains is located at the bottom, the door will now be hinged on the Left side (open from the right to left).

NOTE: The above is the standard design and CANNOT be changed or ordered differently

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings