Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the replacement trim clamps for the obsolete NA1B panelboard?
Issue:
Need the replacement trim clamps for the obsolete NA1B panelboard?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Circuit breaker panelboards sold and supported in the USA.

Resolution:
It is the PK1TC, but it is obsolete with no replacement.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings