Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the torque on the bolt ( I-line 1 busway or joint pack for I-line II) for I-line bus duct?
Issue:
Torque on the bolt ( I-line 1 busway or joint pack for I-line II) for the I-line bus duct.

Product Line:
I-Line Busway

Environment:
I-Line Busway Torque Values

Resolution:
It is 70 lb-ft, +/- 10 lb-ft.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings