Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the cost of fungus proofing for panelboards?
Issue:
Fungus proofing for panelboards.

Product line:
Circuit breaker panelboards sold and supported in the USA.

Environment:
Damp/wet environment

Cause:
Application

Resolution:
Fungus proofing is available for circuit breakers but not  panelboards. The price adder for the circuit breakers is 20% per the Supplemental Digest 177, Page 3-15, Table 3.47.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings