Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How many LP9501 trim clamps are needed for a panelboard?
Issue:
LP9501 Trim Clamps how many are needed on a Panelboard?

Product Line:
Panelboards

Environment:
NQ, NF, ILine Panelboards

Resolution:
The number required depends on the type and size of the panelboard trim. (8 maximum) The LP9501 contains (1) trim clamp assembly.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings