Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the ground fault function be defeated for primary injection testing on PowerPact P frame breakers?
Issue:
Is there a way to defeat ground fault on the Powerpact P-frame breaker for primary injection testing?

Product Line:
Powerpact P-Frame Circuit Breakers

Resolution:
There are two ways to defeat ground fault on the PowerPact P frame breaker. The hand held test kit and full function test kit can be used to defeat ground fault. If neither of these devices are available, the looping method will have to be employed while testing. See FA265488 for explanation of looping method.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings