Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
​Is there an enclosure for the EDB breaker?
Issue:
Do the EDB, EGB and EJB breakers have an enclosure available?

Product Line:
Circuit Breakers

Environment:
Applies to EDB, EGB and EJB circuit breakers

Resolution:
No, EDB, EGB or EJB breakers are designed for the NF panel board only
Consider these instead:
  • 1,2,3,4 pole breakers up to 125A - Powerpact B breaker with its respective enclosure
  • 2,3 pole breakers up to 150A - Powerpact H breaker with its respective enclosure
For more information, go to the Schneider Electric US Home Page, search for "DigestPLUS Online Catalog", and look for circuit breaker enclosures in section 7.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings