Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the standard lug kit for FA/FH breakers?
Issue:
What lugs come as standard on FA breakers

Product Line:
Circuit Breakers

Resolution:
FA/FH breakers from 15 to 30 A: AL50FA  - accepts (1) 14-4 AWG copper or (1) 12-4 AWG aluminum
FA/FH breakers from  35 to 100 A:  AL100FA - accepts (1) 14-1/0 AWG copper or (1) 12-1/0 AWG aluminum

Note: AL50FA may be used as optional lugs for 35 to 100 A FA/FH breakers and AL100FA may be used as optional lugs for 15 to 30 A FA/FH breakers.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings