Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a PAK75CTG, series E03 and E04 ServicePak power outlet panel?
Issue:
What are the replacement parts for a PAK75CTG, series E03 and E04?

Product Line:
Power Outlet Panels

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4054025101
Cover Mounting Screws - 2142717161
Interior Trim - 4054024502
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4054020251 (base assembly not included; breakers and receptacles included)
Base Assembly - 4054008650
Circuit Breakers - QO120GFI, QO130, and QO250
Receptacle - 4054001450 (125 volt/20 amp), 4054004450 (125 volt/30 amp), and 4054027950 (125/250 volt/50 amp)
Receptacle Mounting Screw - 2190312160 (2 required for the 125 volt/20 amp receptacle)
Receptacle Mounting Spring Clip - 2330100001 (2 required for the 125 volt/20 amp receptacle)
Receptacle Mounting Screw - 2159412120 (3 required for the 125 volt/30 amp receptacle; 2 required for the 125/250 volt/50 amp receptacle)
Ground Bar - 4023089855
Ground Bar Mounting Screw - 2159414220
Neutral Assembly - 4054008751
Note: Covers and interior trims do not have labels applied.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings