Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What quantity and size of conductors will a GTK03 ground bar accept?
Issue:
What is the wire data information for GTK03?

Product Line:
Load Centers

Resolution:
This equipment ground kit has 2 terminals and each terminal will accept (1) #14 - #4 AWG or (2) #14 - #12 AWG copper conductors, or (1) #12 - #4 AWG or (2) #12 - #10 AWG aluminum conductors. The ground bar is 1.05 inches long.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings