Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How do you get remote operation on an NW breaker?
Issue:
What parts are needed to be able to remotely operate the NW breakers?

Product Line:
Masterpact NW Circuit Breakers

Resolution:
The breaker would need to have a spring charging motor, a shunt trip, and shunt close to be remotely charged, opened, and closed. To be able to remotely reset the breaker after a fault, an automatic reset (factory installed only) or electrical reset would also be required. The motor, shunt trip, shunt close, and electrical reset would all require control voltage.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings