Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What does the T suffix mean in a QO load center catalog number?
Issue:
Define suffix T in a load center
Product Line:
Load Centers
Resolution:
The T designates that an equipment ground bar is factory installed in the load center as a standard feature.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings