Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the power cable length of the XCMA102?
Issue:
Identifying the cable length of a device

Product Line:
Limit Switches

Environment:
OsiSense XC standard

Cause:
Product Selection

Resolution:
One meter (39``) is standard. For other cable lengths, add the length in meters as a suffix at the end of the part number. For example, XCMA102 with 2 meters of cable is XCMA1022.,

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings