Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Will ground fault alarm work on a generator breaker configured for modified differential ground fault MDGF to sum the currents correctly?
Issue:
Will a breaker using MDGF still be able to signal the ground fault alarm on the M2C/M6C contact through the trip unit?

Product Line:
Molded Case Circuit Breakers

Resolution:
Yes. The signal from the MDGF module is correctly interpreted by the P and H trip units to signal a ground fault alarm through an M2C programmable switch module.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings